The Interactive Learning Poster accompanies the use of the Bionics Kit in the classroom.
The poster guides the learners through the construction of the three robot animals (fish, elephant, chameleon) and provides additional background knowledge, which is conveyed with the help of online learning content. QR codes are used to access the digital content. Thereby the learners come into contact with 3D animations.
After a successful assembly, the learners see virtual robot animals via Augmented Reality. The learners use their own mobile devices. Thus, the interactive learning path is an optimal tool to combine analog and digital learning in a playful way. It helps to use digital tools in the classroom in a meaningful way and is therefore a perfect addition to any integrative STEM educational program.
In order to use the Interactive Learning Poster in a meaningful way, a Bionics Kit is required. Wifi is needed as well.
core range