With the pneumatic starter, students discover how the four disciplines connect as they understand how pressure and force is related and calulated, how pneumatical components work, how they are arranged in circuits and how they are designed to fullfil given technical tasks.
Children cannot start learning about technology early enough. The Pneumatics Starter is an ideal way to begin learning about technology from age 11 onwards.
The Pneumatics Starter deals with a variety of material, from the basic principles of physics (pressure, force) through to logic operations and the basic principles of automation technology. It uses only authentic industrial components, which helps to ensure high motivation on the part of students. Students can discover the purpose of components for themselves and use them to assemble interesting circuits.
A further special feature is the opportunity for hands-on experience of the components – for example, the air supply for the Pneumatics Starter is provided by a small hand air pump and reservoir. This directly demonstrates to students the relationship between pressure and force.
Additional advantage - working with the Pneumatics Starter is absolutely safe.
Science
Technology
Engineering
Math
Detailed documentation on CD-ROM (de/en/es/fr): Comprehensive book of exercises with solutions and didactical instructions for use in teaching; companion materials with numerous colour illustrations, basic representations, photos and sectional views and safety instructions, including copying rights
core range