This problem shouldn’t occur. If you are not able to establish a connection between the controller and your mobile device follow these steps:
If your device is connected to the Wi-Fi of the Bionic Flower but you can’t open the website inside your browser please try following steps:
Make sure that the external sensors are correctly connected. Both connectors on the application board and the sensors are labeled with rectangles. The black cable of the sensor cable must be connected to the black rectangle of the sensor and to the white rectangle of the application board.
Unplug the Bionic Flower to switch off the control unit and reconnect the sensors after turning the Bionic Flower on again.
The network name of the Bionic Flower is printed on the ESP32: “b4e_XXXX” –(XXXX stands for the individual network name). You can also scan the QR-Code attached on the ESP32 for a direct automatic connection.
We always improve our software. Check the latest software version on GitHub. Here, you can find the flash file with the latest software of the Bionic Flower.
Instruction
Unpack the ZIP file. Connect the control unit to the PC using the USB cable. Start the batch file and follow the instructions. The microcontroller is flashed with a new code and should work afterwards.
If you have problems executing the batch file, please execute it as administrator. To do this, right-click on the batch file and select “Run as administrator” from the menu. If you have administrator rights, you can execute the file without any problems. If you still have problems, please contact us via our contact form.
The password is “education”.
Yes, the Bionic Flower can be controlled with your own smartphone. A connection between the control unit and the mobile device must be established.
No, a native app is not required to control the Bionic Flower. The control interface appears in the browser of your device.
The control unit provides its own Wi-Fi hotspot that you can directly connect your mobile device with. Wi-Fi is only needed if you want to access the teaching materials via the webpage.
You can find a “Burger” menu in the upper left corner of the website. In the “burger” menu you can switch between two modes:
Once you established a connection with the control unit via Wi-Fi and opened the website “www.b4e.de" or “192.168.4.1” a webpage appears with sliders. It is best to tap on the point on the slider where you want it to be moved. Otherwise you can also slide it.
No, there is no stop button. You can stop the movement by moving the slider to zero or just unplug the Bionic Flower from the power supply.
The microcontroller used is the ESP32 Dev Kit (v4). It is compatible with the Arduino programming language.
The microcontroller comes pre-lashed and is ready to use.
Yes, the code of the Bionic Flower is open source. You can find the source code of the Bionic Flower on GitHub.We provide it free to use and to modify.
Before you can load a modified source code to the microcontroller, you need to download the Arduino Portable version from our website. All necessary libraries and settings are preset, so you don’t need to do a complicated installation and can start right away. On instructions we have also included some first program examples, so you can learn directly how to control the Bionic Flower yourself.
Some of the CAD data are available on our website.
The white paper leaves we provide in our kit are suitable for single use. You can also download a template from our website to make your own new leaves. You need to print this template on a thicker paper such a cardboard. You can also design your own leaves with a individual shape and color.
The length of a lesson depends heavily on how deep you dive into the topic and the age of the pupils. You can use the flower for a short intro lesson where younger students just create some new leaves (app. 30 -45 min), you can have the students assemble the flower from scratch (60 – 90 min), make experiments with the sensors (45 -90 min) or let the students create new behavior of the flower by programming it with Open Roberta or C++ (90 min to several days).
Yes, teaching material is on our website. A special teacher handbook is currently being developed.
An elaborated online course with background knowledge for the Bionic Flower is available for free on our learning platform Festo LX. Here you have to create a free account in advance.
Up to four students can work on one Bionic Flower construction kit.
The Bionic Flower covers different topics from biology (e.g. sensors and actuators in plants, folding structures), technology (e.g. sensors (touch, light), actuators (stepper, LED), control technology, programming in Scratch and C++, light and colors), project management and creativity and art.
In principle the flower can be assembled and disassembled many times, nevertheless we do not recommend it. All of the learning content can be covered with the fully assembled flower.
The leaves, however, can be colored and folded by the students. If you wish to use fresh leaves for every course, we offer prepunched leaf sets. You can also use the punched out cardboards as a template to create new leaves on your own or download the template of our leaves on our website.
No, in effort to become more sustainable we are moving from printed to online materials such as our assembly instruction. Please feel free to print the assembly instruction if you want to have a paper version.